4/15/2008 3:04 PM | |
Posts: 11 Rating:
|
Hello, I need help with my program that I am trying to write. What I have is a conveyor that will dispence parts from a staging area. I need to supply 2 lathes from here. When I see that my system is empty at all areas, then I want to release 6 parts to the furthest lathe. When I see that the system is filling then I want to extend a gate and individually release six parts to the other lathe. After this I will see that I need to send parts to the furthest lathes magazine. I want to send 15 parts to fill it. Then the process will send parts as needed to either lathe. I am attaching my program that I have so far. I also want to know if there is a feature that allows mw to only run a part of the program when between to instructions. I would like to have each parts request run asif it where its own program ignoring the other parts request untill the current parts request isbeing fullfilled. Also is there a function similar to what allen bradley does with thier mcr instruction. All yourhelp is appreciated.
Attachment1020_23_rev.1 April 12,2K8.zip (251 Downloads) |
Follow us on