(1)| 5/15/2009 10:53 AM | |
|
Posts: 9 Rating:
|
Hello I am trying to get connection between old Telemecanique TSX47-411 (or TSX 87-425) with Siemens HMI. Protool and WinCC Flexible manuals say that it is possible using Unitelway bus and SCA62 junction box. But manual 6AV6596-1MA06-0AB0 (Communication for Windows-based Systems: Part 2, page 18-2) says: " For connection of the operating unit, an RS 485 interface card configured as follows must be used: - Rx: always on - Tx: controlled via RTSTests performed by Siemens AG involved the use of interface cards of the type C102, CI 132, CI 132I or Ci 132IS from Moxa Data Communication Solutions." Attachmentcomb2V6_e_18_2.pdf (300 Downloads) |
| 5/26/2009 10:51 AM | |
|
Joined: 5/8/2006 Last visit: 10/23/2025 Posts: 1085 Rating:
|
Hi You need this cards with RS485 interface for PCs. Bye |
| 6/15/2009 8:45 AM | |
|
Posts: 9 Rating:
|
Hello Hristo For comunication with TSX I used TP170 panel with ProTool application, probably you may use WinCC for that purpose. 1) First off all you need to get SCA62 passive junction box, which is just a box with two internal connections and two external for non-telemecanique devices (you can set unitelway address). 2) Prepare cable (details in attachement). 3) Make a ProTool application: - set apprioprate controller in 'Bus Module / CPU Type', - 'Telway 7' set No Network - 'Gate' if you use CPU with built-in Unitelway port you have to set 'System' (I use TSX 87/425 with build-in Unitelway port, so that is why I have chosen Gate->System) - 'OP Interface' is set automatic - 'OP Unitelway Station' you have to check which address is free in your network Remember, if you use CPU with Unitelway port, you have to be sure the address is set to 0. Than you create tags similar to Siemens tags, you just set different memory area (set attachement). After all download the project to your HMI. Connect HMI to SCA62 box and then power up HMI. What I noticed sometimes I loose connection between TSX and Siemens HMI and I do not know why, so at this moment it is very unstable and I treat it just for tests. I you find any problems do not hesitate to contact me. Best regards, macio Attachmentunitelway.zip (298 Downloads) |
| 6/15/2009 12:50 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello macio, Thanks and excellent! Best regards Hristo Mihalev |
Follow us on