(0)| 9/2/2016 2:52 PM | |
|
Joined: 6/3/2014 Last visit: 1/21/2026 Posts: 660 Rating:
|
Hello himarele, I think it should be possible with a script. If you change the location with tags, then you can use C or VBS. Here is an example and a reference for the dynamization of objects with VBS:
Example code added to Facplate "Properties > Events > Click" which would move the faceplate to the upper left Corner of the Screen. Instead of "0" you can use the SmartTags for the coordinates.
On a PC you can use Windows API function to read the mosition/coordinates of the mouse. You need to use a C script for that. I didn't try it myself yet, so I don't know if it works well enogh.
|
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on