(4)| 9/17/2016 1:55 PM | |
|
Posts: 8092 Rating:
|
It depends on application. If any one motor is required to run at a time, you can have single drive & by configuring different DDS you can select the motor you want to run. MICROMASTER: Working with different drive data sets DDS / command data sets CDSIf your application demands more than 1 motor to be run simultaneously, you need to select appropriate drive. HTH |
| 9/17/2016 3:07 PM | |
|
Posts: 4 Rating:
|
ok, in one of this page speak about the posibility to change de motors parameters, this include the diferent powers? whitch is the range for the same vdf to drive a diferent powers? siemens have a software or a paper to see this? |
| 9/17/2016 3:44 PM | |
|
Posts: 8092 Rating:
|
Yes possible. Only one CPU unit & select PM of higher capacity e.g. suitable for 37 Kw motor rating. |
Follow us on