(0)| 10/10/2016 2:44 AM | |
|
Posts: 27 Rating:
|
Hi, I have problem with Modbus Server CP S7 400, by CFC.
the Hardware NET PRO is right. 1 1FFE. port 502 I try to connect by MODBUS SCAN software to the PLC, Dont have conection and try with the Wincc driver MIODBUS Premiun Micro, the answers It is Same dont have conection to the server.
Please is anyone have a configuration of SERVER Modbus TCP. My hardwares is only one side of the S7412H, I think that is no the problem, and i am try with the demo licence of the MODBUS I have the OB121. attached some picture to see more, thanks for your attention. ------------------------------------------------------------------------------------------ AttachmentModbus TCP Issue.docx (518 Downloads) |
Last edited by: RenatoAlex at: 10/10/2016 2:44:44 AMLast edited by: Min_Moderator at: 10/10/2016 4:05:05 PMNew subject after splitting |
|
| 10/10/2016 2:40 PM | |
|
Posts: 57 Rating:
|
Hi RenatoAlex When you try to communicate with the simulator, have you checked the connection in NetPro? Is it connected or does it wait for a connection? A0FF means that connection is currently not ready for communication and that you should check the connections. If applicable correct the value at check_conn_cycle. The error can also occur when a CP is used that does not support AG_CNTRL. |
Follow us on