(2)| 10/31/2016 11:13 AM | |
|
Joined: 4/24/2006 Last visit: 1/15/2026 Posts: 9105 Rating:
|
Hello, Have you seen this link: Discontinuation of SIMATIC MP 270B 6" Touch What is the MLFB number of MP270B? (6AV.....) Best regards, Wizard |
This contribution was helpful to
|
|
| 10/31/2016 12:04 PM | |
|
Posts: 4620 Rating:
|
Hello AutoGen_8970706, Other link with also MP 270 10" Discontinuation: SIMATIC TP 270, OP 270 and MP 270 Pay attention also the MP 277 is in Phase Out End of Production for SIMATIC MP 277 Panels with Narrow Frame - ID ... Modification at Short Notice: SIMATIC MP 277 8" / 10" Touch and Key ... and important you have original project? If not no way to change panel you have to buy the exact type of panel so another MP 270 |
Follow us on