11/9/2016 10:31 AM | |
Posts: 4 Rating:
|
Hello, Has anyone used the limit switches successfully in this kind of application? Or used the drives in a similar application? |
11/15/2016 6:23 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Could you please tell us which DI are configured for limits & which parameters are set? |
11/17/2016 1:47 PM | |
Posts: 4 Rating:
|
Hello, The CWL limit is configured to input 3 and the CCWL limit is configured as input 4. I have attached a screenshot and a project file so you can see it. I think/hope this is set correct. AttachmentDI.zip (440 Downloads) |
Follow us on