(0)| 4/29/2008 4:17 PM | |
|
Posts: 4 Rating:
|
Dear Mr.Bell: Thank you very much for your attention, the PING time from component to another is about 5 ms. |
| 4/29/2008 5:03 PM | |
|
Posts: 4 Rating:
|
Dear Mr.Bell: Thank you for your advise, But actually , In the application, there aremore than 10 components in the workshop,in order tomanage the netwrok, the customer have build up difference logic netwrok for differenct fuction section , so, they need use Cbacomponents in difference logic network. and acorrding to your statement,it is not so good use Cba solution in the application, so, if I use the OPEN TCP connection as you mention before (Generating the Connection Data for the open TCP/IP Communication using the Open Communication Wizard http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=25209116&caller=view) canthe response timebecome shorter? andif I use a PC ping the PLC located in the difference logic network, the PING time will be 5 ms, it is true, B.R Wangw eiliang |
Follow us on