(0)| 4/23/2008 3:47 PM | |
|
Posts: 559 Rating:
|
Respected all, I made new project in Step-7 with Cpu 412-3H. I added Hmi station in project. Now when I open Wincc Flxible Project throgh Step 7 project. than it opens And One message in Output of flexi comes" Symbol Server has encountered a problem".As per attached file. than I saved and opened project again from step 7. After I make on the connection of 2 Cpus in Wincc Flexible and Saving the project again It stops at one stage "Saving S7hmi project". I waited for more than 15 min. But Still there was no progress. So please help me to correct this problem It is very urgent for me. I have Step 7 V 5.4+sp3+hf1 and Wincc Flexi 2007. Attachmentfault.zip (152 Downloads) |
| 4/24/2008 12:24 PM | |
|
Joined: 5/8/2006 Last visit: 10/23/2025 Posts: 1085 Rating:
|
Hi, you should install the HF4 for WinCC flexible 2007. Here is the link: http://support.automation.siemens.com/WW/view/en/28882233 Bye |
| 4/27/2008 12:35 PM | |
|
Posts: 559 Rating:
|
Thank u. I found the solution through Wincc flexi 2007+HF4. |
| 5/4/2008 5:51 PM | |
|
Joined: 9/7/2007 Last visit: 4/3/2025 Posts: 550 Rating:
|
be sure to revise the compatibility of the soft wares it is so important |
|
Best Regards |
|
Follow us on