(0)| 5/2/2008 1:59 PM | |
|
Posts: 5 Rating:
|
Attached is very crude sketch of my application. It shows an elevation of a elevator hoistway with 6 floors (landings). It also shows the elevator car at the bottom landing. My application actually has 15 floors. So, the main controller (home of ASi master/psu) is above the elevator hoistway in the machine room. There are two ASi legs coming from the machine room. The 1st leg is 18ga unshielded that services 15 landings with one 4I/O slave at each landing. The 2nd leg is 18ga shielded elevator travel cable that services the elevator car which has two 4I/O slaves. Both legs are approx. 300ft. each. The Lowest slave on leg 1 has an extension plug. I have no repeaters or extenders in this configuration. Thanks. Rick AttachmentElevator_Sketch.pdf (558 Downloads) |
Follow us on