(2)| 6/9/2007 3:49 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Marques, Of course that is possible, you can do it only on different ways like the two other answers represent. See the manual Communication with SIMATIC for more information about the communication, for instance with TCP. Please see the manual Commissioning PC Stations - Manual and Quick Start to read something about this communication with SIMATIC NET and OPC. You may find also in the next manual a lot of information Industrial Communication with PG/PC Volume 2 - Interfaces Programming Manualabout communication. When you have a PN-CPU then you can use the TCP/IP wizard which is describedin the Application & Tools part: Generating the Connection Data for the open TCP/IP Communication using the Open Communication Wizard |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
| 6/12/2007 8:30 PM | |
|
Posts: 126 Rating:
|
Thanks J_Bell for your reply,well i have to decide what to do now. Best regards to you all, Marques |
Last edited by: Marques at: 13.06.2007 10:18 |
|
Follow us on