(0)| 5/6/2008 2:01 PM | |||
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello manc; Since USS runs on a RS-485 layer, maybe you could look at the active termination node used for Profibus-DP. You have to provide 24 V DC to the unit in the fiield for it to function; it is installed in the field, din-rail mounted.
Daniel Chartier |
||
Follow us on