(0)| 1/27/2017 7:48 AM | |
|
Posts: 8092 Rating:
|
How you interfaced encoder with S120? |
| 1/30/2017 12:24 PM | |
|
Posts: 115 Rating:
|
thanks for the answer, regarding to the encoder, mine is erm 180 wich is a incremental 1 Vpp encoder so i think that with the SMC 20 should be working. |
| 1/30/2017 12:50 PM | |
|
Joined: 5/12/2006 Last visit: 1/21/2026 Posts: 22829 Rating:
|
but he use a ERM180! |
This contribution was helpful to
|
|
| 1/30/2017 12:52 PM | |
|
Posts: 115 Rating:
|
I apreciate your help but...
PD: THANKS CRISTOPH!! AttachmentData Sheet AK ERM 18.pdf (182 Downloads) |
Last edited by: mikellass at: 1/30/2017 12:53:11 PM |
|
| 1/30/2017 12:53 PM | |
|
Joined: 10/11/2006 Last visit: 1/21/2026 Posts: 6072 Rating:
|
Hello, I guess the errorcode is clear. You get no Zero mark.. Please check the manual of the encoder and your settings and wiring. When you are no successful, please contact the hotline. Support Request :http://www.siemens.com/automation/support-request F31101 (N, A) Encoder 1: Zero mark failed Message value:%1 Message class:Actual position/speed value incorrect or not available (11) Drive object:A_INF, B_INF, ENC, HLA, R_INF, S_INF, SERVO, SERVO_AC, SERVO_I_AC, TM41, VECTOR, VECTOR_AC, VECTOR_I_AC Component:Encoder 1Propagation:LOCAL Reaction:Infeed: NONE (OFF1, OFF2) Servo: ENCODER (IASC/DCBRK, NONE, OFF1, OFF2, OFF3, STOP2) Vector: ENCODER (IASC/DCBRK, NONE, OFF1, OFF2, OFF3, STOP2) Hla: ENCODER (NONE, OFF1, OFF2, OFF3, STOP2) Acknowledge:PULSE INHIBIT Cause:The 1.5 x parameterized zero mark distance was exceeded. The zero mark distance for the zero mark monitoring is set in p0425 (rotary encoder) or p0424 (linear encoder). Fault value (r0949, interpret decimal): Number of increments after POWER ON or since the last zero mark that was detected (4 increments = 1 encoder pulse). See also: p0491 (Motor encoder fault response ENCODER) Remedy:- check that the encoder cables are routed in compliance with EMC. - check the plug connections. - check the encoder type (encoder with equidistant zero marks). - adapt the parameter for the clearance between zero marks (p0425). - if message output above speed threshold, reduce filter time if necessary (p0438). - when p0437.1 is active, check p4686. - replace the encoder or encoder cable. |
|
With best regards, |
|
This contribution was helpful to
|
|
Follow us on