(0)| 2/16/2017 11:38 AM | |
|
Posts: 112 Rating:
|
Dear All, How do I upload program from MP377 HMI. Is it possible? Or Do I have to have the original back up? Regards Satheesh |
| 2/16/2017 11:41 AM | |
|
Joined: 5/12/2006 Last visit: 1/19/2026 Posts: 22806 Rating:
|
Hi, Uploading only possible, if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable backtransfer". So if the option was set then yes, if not then no. https://support.industry.siemens.com/cs/ww/en/view/21907703 Regards |
This contribution was helpful to
|
|
Follow us on