(0)| 2/16/2017 12:43 PM | |
|
Joined: 4/28/2015 Last visit: 6/29/2020 Posts: 3 Rating:
|
Application : Tower crane We are using Sinamics G120(PM240-2, 6SL3210-1PE31-8AL0) + DBU(6SE7032-7EB87-2DA1-Z M08). During hoist down, the capacitors in DBU are heating up. Very hot, and actually one DBU was blown(capacitors got blown). When we trace the dc link voltage of the drive at hoist down, the voltage fluctuation is around 100Vdc, very severe. When we put the DBU to S120, it is well working.. As we know, the major difference between S120 and G120 is internal dc reactor. What is the root cause of the trouble? AttachmentDBU trace.pdf (227 Downloads) |
Follow us on