(0)| 3/2/2017 6:11 PM | |
|
Posts: 3 Rating:
|
Hello Again, I am having an issue with viewing an oscilloscope interface using the a TP1900 Comfort Panel HMI. I am using a TP1900 Comfort Panel HMI (6AV2124-0UC02-0AX0) with an the operating system that is Microsoft Windows CE 6.0. I am trying to use the HMI to view a web-based oscilloscope control interface. The oscilloscope a Keysight DSO6014L rack mount and it uses a standard Java-enabled Web Browser. On the HMI Comfort Panel, the version of WinCC Runtime that is installed is V13.0.0.5. In the WinCC Runtime project on my configuration PC (which is using TIA Portal V13 SP1 Basic) I am using the Sm@rtClient Viewer with an IP address of 192.168.0.11 non-encrypted. This is the same IP address that I have set up on the Keysight oscilloscope above. When I install the program from my configuration PC onto the HMI Comfort Panel and then run the program on the HMI, I can only view the waveforms. I CANNOT view the actual control menus for the oscilloscope. When I connect to the oscilloscope using my configuration PC, a java window pops up and I can see the control menu and the waveform. Since the HMI Comfort Panel operates on Microsoft Windows CE 6.0, am I able to install java onto this device? I am running into issues having .exe applications run on the HMI. Does the version of WinCC Runtime that is on the HMI (V13.0.0.5) even support java-enabled websites? Or should I set up the HMI device as a Sm@rtServer? If someone could please help me out that would be great. Thank you in advance. |
Follow us on