(1)| 5/6/2008 8:17 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Dear Prash, Which driver do you use on the CP1613 (A1) side ? Please consider that if you are using a SIMATIC NETS7-1613driver that it would be a very expensive connection, the driver wanted to keep always contact.... It is better to built up the connection, transport your data and then closing the connection, or do you want to communicate always ? MODBUS on TCP/IP is also possible, then you need a functionblock from I&S www.siemens.com/IT4Industry AttachmentOpen_Modbus_TCP.pdf (545 Downloads) |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on