(0)| 3/20/2017 5:49 PM | |
|
Posts: 8 Rating:
|
Hello, I am also having this issue on a CPU 319-3 PN/DP. Details below: -------------------------------------------------------------------------------------------------- Parameter assignment error preventing startup in CPU module parameters --------------------------------------------------------------------------------------------------- Some things that I've tried to alleviate the error are checking HW config part numbers vs. actual part numbers, making sure modules are screwed down tight, checking the backplane and cpu/cp back connector, etc. The odd thing is that online HW config diagnostics show that no modules are in error, only the CPU with the message above. Also, we do not have an 'output 520'. There is only one AQ card configured with addresses 512-519. Thanks for advice. ------------------------------------------------------------------------------------------ |
Last edited by: loftedspace at: 3/20/2017 5:50:47 PMLast edited by: Min_Moderator at: 3/21/2017 2:32:13 PMNew subject after splitting |
|
Follow us on