(0)| 4/4/2017 12:57 PM | |
|
Joined: 5/12/2006 Last visit: 1/16/2026 Posts: 22804 Rating:
|
Hello, what do you mean with "material"?
Christoph |
| 4/4/2017 2:32 PM | |
|
Joined: 4/28/2015 Last visit: 11/27/2025 Posts: 10970 Rating:
|
Hello, |
|
With best regards... |
|
| 4/4/2017 6:06 PM | |
|
Posts: 4620 Rating:
|
Hello, some infos: What master/slave communication options are ... - Siemens Support How can you communicate data between the S7-200 and the S7-300 via PROFIBUS DP? how to configure s7-300 and s7.1200 ... - Siemens Support but if you explain better what you want to do........ |
This contribution was helpful to
|
|
| 4/5/2017 2:53 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Bil; I am sorry, you are going to have to show more precision whn you come to the forum and ask for help. For example: - The CPU 314 you mention cannot be a Profibus-DP master (without a CP 342-5), unless you mean a CPU 314C-2DP; provide the complete part number please. - There is no IM 151-C in Siemens equipment, unless you mean an ET 200S head module (IM 151-1, IM 151-7...); what is the complete part number (again) of the Profibus slave you want to connect? -Are you using Simatic Manager (what version, 5.x) or TIA Portal (what class of Step 7. Basic, Advanced..., and what version, v13, v13.1...). Note that Stefano (STE39) has already provided interesting links that can provide guidance in setting up a S7-300 CP as Profibus master and another CPU as a slave. For my part I can propose a section of the Siemens programming tutorials (in Word format), one that deals with the configuration and data exchanges of a CPU 314C-2DP master and a IM 151-1 slave: Modul_D16 - SiemensHope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/5/2017 3:29:51 PM |
|
This contribution was helpful to
|
|
Follow us on