(0)| 4/25/2017 4:32 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Simpist; What protocol do you plan to use between the Sentron PAC4200 and the Siemens PLC? You require a gsd file to setup a Profibus-DP slave in a Profibus master's configuration. If this is what you are trying to do, then you need an expansion module for Profibus-DP on the Sentron PAC 4200; then the gsd file for Sentron units will be useful. See the following discussion: If you wish to connect to the Sentron through Modbus/TCP then look at the information in the following discussion (you will find a sample project in that thread): comunications between S7-1200 and the Sentron PAC4200's on ModBus/TCP Ethernet Hope this helps, |
Last edited by: dchartier at: 4/25/2017 4:33:40 PMLast edited by: dchartier at: 4/25/2017 9:15:05 PMLast edited by: dchartier at: 4/25/2017 9:15:41 PM |
|
Follow us on