(0)| 5/24/2017 9:08 PM | |
|
Posts: 1 Rating:
|
I need to communicate 8 VFD G120 (CU240E-2 PN) to a basic panel KTP700, it is posible? how many I/O devices can connect directly? Thanks a lot. Best regards. |
| 5/25/2017 6:44 AM | |
|
Posts: 387 Rating:
|
Hello, Did you see this application example? I think you should consider using PLC if all the drives are to be operated simultaneously. You can connect 8 drives to HMI but you cannot operate all at the same time. You have to use 'change connection' in HMI as explained in the example, to changeover between drives. Hope this helps. Kbv. |
Follow us on