(0)| 5/27/2017 4:17 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello jack_lohana; There were no available Modbus (RTU or TCP) channels in WinCC v6 provided by Siemens.There was a Modbus RTU channel in v5.2, but it was developped externally by Allmendinger, and it did not renew its partnership with Siemens as per version 6 of WinCC. At this time, you could buy a license for Modbus TCP (or RTU) directly from Allmendinger, which can be integrated in WinCC v6. See the following link (and check the supporting OS versions of Windows): The other option would be to use your PLC to exchange as a client over Modbus TCP with your server, and transfer the data to WinCC through the integrated channels of WinCC 6: MPI, Profibus, Ethernet. See this discussion, based on a Siemens PLC: https://support.industry.siemens.com/tf/WW/en/posts/modbus-tcp-driver/29250?page=0&pageSize=10 Hope this helps, Daniel Chartier |
Follow us on