(0)| 7/4/2017 12:00 PM | |
|
Joined: 10/11/2006 Last visit: 1/21/2026 Posts: 6052 Rating:
|
Hello, you can use the BOP-2 or the IOP to configure drive parameters. If you want to copy the parameters from the old CU to the new one you can use the BOP-2 or a memory card. You can find further information about saving settings and series commissioning in the operating instructions of the used CU, for example in section 7 of the operating instructions of CU240E-2 https://support.industry.siemens.com/cs/ww/de/view/109744796/en?dl=en As long as the new CU have the same firmware versions there will be no issues. I would recommend using a memory card for parameter transfer. There you can store the firmware too, so the new CU will be up-/downgraded to the corresponding firmware version if the memory card is inserted and the CU is powered up. |
|
With best regards, |
|
This contribution was helpful to
|
|
Follow us on