(3)| 6/7/2010 10:35 AM | |
|
Posts: 19 Rating:
|
Dear experts I need analog output 0-10v at terminal 13 &14 (Micromaster440). Which parameters are to set for this application. Thanks Haque |
| 6/7/2010 11:49 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, You meant terminal 12 and 13. Look at attachment. Perhaps Operating Instructions (Compact): MICROMASTER 440 is useful. Best regards, Hristo Mihalev |
| 6/7/2010 1:05 PM | |
|
Posts: 19 Rating:
|
Dear UMENCHO Thanks for ur reply. Best regards Haque |
| 6/8/2010 8:40 AM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
I am sorry but experts might have over looked your question. DIP Switches are for Analog Inputs not for Outputs For 0 to 10 V AO, you have to set 1 in P776 and set other parmetrs as suggested by RBM You must connect 500 Ohm resistor between Terminals 12&13 for AO1 and between 26&27 for AO2 Please Refer Parameter List manual for More details. Have a look to attached file Regards, Devesh AttachmentCopy of 440_PLi_23708204_en_0106.pdf (978 Downloads) |
Last edited by: Vithani at: 6/10/2010 11:02 AMI dnt mind if you give rate in addition to thanks....;) I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
| 5/17/2016 11:27 AM | |
|
Posts: 4757 Rating:
|
New question published by sharif s is split to a separate thread with the subject Read the frequncy from drive. Best regards |
| 7/25/2017 6:59 AM | |
|
Posts: 8171 Rating:
|
New question published by yaseen.patel7 is split to a separate thread with the subject How to set 4-20ma current output from AO. Best regards |
Follow us on