3/7/2006 6:14 AM | |
Joined: 3/2/2006 Last visit: 7/15/2008 Posts: 29 Rating:
|
Hi We are using the WinCC 6.0 SP3 Asia on one of our projects. But, in this project, we are using two monitors. The graphic controler (display card) we are using is one Leadtek (www.leadtek.com). Now, we have this problem: when we open a ComboBox pop up on the left side of the screen (first monitor) the pop up works fine; when we use the same pop up on the right side of the screen (second monitor), the pop up is shown on the left side again! You can see it clearly on the attached file. Do you know this behavior? Do you know some graphic controler that can handle this problem on the best way? Thanks, Paulo Attachmentleftside.zip (681 Downloads) |
3/7/2006 10:10 AM | |
Posts: 3149 Rating:
|
Hi, you should normally just use those graphic cards, which can be orderedin your WinCC/PCS7 catalogue. http://support.automation.siemens.com/WW/view/en/7727705 http://support.automation.siemens.com/WW/view/en/14564777 http://support.automation.siemens.com/WW/view/en/831486 In your Windows-system settings you can normaly choose the prefered screen. Nemo |
Follow us on