(0)| 8/24/2017 8:10 AM | |
|
Posts: 66 Rating:
|
Hello Friend , I made this sample project to test how the SINAMICS G110 works with USS protocol , but i found my program not working, i changed the following parameters in the G110 as recommended, may anyone please tell me where is the problem . Thank you in advance. G110 configuration : USS Address= P2011 = 0 USS Baud Rate =P2010 = 6 = 9600 bps USS PZD Length =P2012 = 2= Two 16 bit words are in the Frequency Setpoint = P1000 = 5 =Frequency demand via USS protocol (HSW) Command Source= P0700 = 5= Via USS protocol (STW) Please download the PLC program (TIA V.11) from the following link : --deleted Link--- AttachmentUSS test.zip (136 Downloads) |
Last edited by: Jen_Moderator at: 8/24/2017 3:02:55 PMAdded File as an attachment. |
|
| 8/24/2017 3:03 PM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice.
|
Follow us on