(0)| 8/23/2017 11:33 AM | |
|
Posts: 2 Rating:
|
Hi there, I read some points which were there, but I could not solve my problem. I am going to dim some lights [SMD] by using LOGO!. The problem is here, - How can I use analog output for dimming? - What is the best solution to convert 0-10 v analog output into 220 v AC? [the lights are 220v AC, does it need to convert with the aim of dimming, or there is other solution or tool?] - Does the dimmed light harmful with respect to the lifetime of the lights? BR,
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 8/23/2017 12:48:19 PMNew subject after splitting |
|
| 8/23/2017 1:17 PM | |
|
Joined: 12/18/2014 Last visit: 1/15/2026 Posts: 36458 Rating:
|
The only solution for dimming 230VAC LEDs is a dimmer for LEDs with a 0/1-10V control Input. |
| 8/23/2017 3:31 PM | |
|
Posts: 13 Rating:
|
Hi, you can use 1-10V as input to DIAC and TRIAC Ckt to convert it. |
Follow us on