(0)| 6/22/2008 1:16 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Torpedo1215a; Here is how Siemens describes communication channels for the Hawkeye 1600T on its Vision portal: Flexible communication options – through to PROFINET IO Apart from the well-proven PROFIBUS DP communication, all cameras also offer PROFINET IO capability for high-performance realtime communication on Ethernet basis. Standard function blocks support easy communication to the PN/PB CPUs of SIMATIC S7-300 and S7-400. Alternatively, communication is possible via TCP/IP to the CPs of SIMATIC S7-300 and S7-400. Standard function blocks also support easy communication here between the camera and SIMATIC S7 PLCs.https://www.automation.siemens.com/simatic-sensors/html_76/bildverarbeitungssysteme_kameras.htm?HTTPS=REDIRAnd here is a link to an application note provided by Siemens: Application note: Hawkeye 1600T to S7-300 over Ethernet (native TCP/IP) http://support.automation.siemens.com/WW/view/en/29128081 |
Last edited by: dchartier at: 6/22/2008 1:18 PMLast edited by: dchartier at: 6/22/2008 1:17 PM |
|
Follow us on