5/12/2017 9:28 PM | |
Posts: 10 Rating:
|
All, I am working on solution to collect the Motor Current data from SIMODRIVE 611 system. The system is very old and the drives are analog drives. The PLC and NCU are combined. I contacted Siemens CS and they asked me to contact TechSolve Inc a Siemens solution partner company. They come up with the Adapter VA-SHA-1.3-0.0 Siemens SINUMERIK 840D w/HMI Advanced MTConnect Adapter. 1. Have any one used this adapter? 2. Does it dependent on Solution Line / Power Line type of the 840D CNCs or it is universal? I read 2 different adapters for NCU and PCU. From what I understand from initial conversation with the customer, they are using old system which has PLC and FM-NC NCU combined. I spoke to Siemens and they said that is very old system.The machine is an CNC machining center with 840D Power-line control. 3. The end goal here is able to transfer the data to the database that they have in their plant. Does this adapter capable of doing this? I read about the MT Connect software. Is it possible to configure MT Connect to communicate with the database? 4. How to interface this Adapter to 840D system? 5. Is there any dedicated config tool to configure this adapter? or is it just a plug and play tool? 6. Does anyone has detailed user manual for this? Thanks, Ashish AttachmentTechSolve VizAdapter Data Sheet - Siemens SINUMERIK 840D w_HMI Advanced MTConnect Adapter.pdf (398 Downloads) |
5/12/2017 9:37 PM | |
Posts: 10 Rating:
|
here is the picture of the System? Thanks, |
Follow us on