(0)| 7/1/2008 8:06 PM | |
|
Posts: 1742 Rating:
|
Hello, To be able to control the device directly via AT commands, use a terminal program, e.g. HyperTerminal. Note the following settings: Make the connection: COM port to which the device is connected Speed: 19200 Bit/s Data bits: 8 Parity: NoStop bits: 1 Duplex: FullI would also check if your cable has the correct pinning. See the picture in annex from the manual: AttachmentMD720-Modem cable.zip (468 Downloads) |
| 7/2/2008 8:28 AM | |
|
Joined: 9/28/2005 Last visit: 12/9/2025 Posts: 2957 Rating:
|
Hello, You must use standard modem cable for that which has all 9 pins used. |
|
Best regards, |
|
| 7/2/2008 9:30 AM | |
|
Posts: 3 Rating:
|
Thanks to everyone. We've solved the problem. It was actually cable related. |
Follow us on