(0)| 10/13/2017 5:26 PM | |
|
Posts: 11 Rating:
|
Will there be an external electronic card to achieve effective communication between them or could it be built? |
| 10/14/2017 3:51 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello trebol; As you see in the proposed table above, an OP77A supports Profibus-DP. If your PLC rack contains a CP 541 you might be able to connect it to the operator panel. CP 541 Communications Processor - Industry Support Siemens The reason that the OP 77B can connect to the S5-103U's porgramming port, which supports AS511 communications, is that it has a RS-232 interface (IF1B) that you can use with a TTY-RS-232 cable (with an addes 25-pin to 9-pin adapter). See for example this video: PC/TTY:cable between computer RS232 port and siemens simatic S5 The OP 77A does not support RS-232 communications, so this solution cannot be used. Hope this helps, Daniel Chartier |
| 10/17/2017 4:27 PM | |
|
Posts: 11 Rating:
|
Muchas gracias por la información. Fue una gran ayuda. |
This contribution was helpful to
|
|
Follow us on