(0)| 10/30/2015 9:00 AM | |
|
Joined: 9/12/2007 Last visit: 7/8/2025 Posts: 12 Rating:
|
Hello, The following is the system architecture: Observation: Meanwhile, the Server 2 (Standby server) is still refresh the data pretty fast. If I stop the Server 1 and Server 2 becomes Active server, the refresh speed back to normal. Now let's say I don't stop Server 1 and copy the swapped out data from Server 1 to 2. And connect the swapped out data then Server 2 behaves the same as Server 1 and refresh rate slows down. If I deactivate and reactivate Runtime, then back to normal. This system just commissioned for more than a week. In my opinion, it shouldn't slow down the system. I've attached the diagnose files of both servers for your reference. I'm looking forward to your advice. Thank you Attachmentdiagnose.zip (150 Downloads) |
Follow us on