(0)| 5/23/2017 12:56 AM | |
|
Posts: 37 Rating:
|
Hi,
Yes, the ethernet port is shared between your arduino sketch and the linux operating system.
The difference is, that you don't have to configure the Ethernet interface (e.g. no need to set MAC, IP, gateway, dns, dhcp). The only header you need is "EthernetClient.h" and the class EthernetClient. See the stripped down example, based on the example sketch "Ethernet (Galileo)/WebClient" in the attached sketch. Michael AttachmentGalileoWebClient-170523a.zip (1587 Downloads) |
Last edited by: turner42 at: 5/23/2017 12:59:03 AM |
|
This contribution was helpful to
|
|
| 11/20/2017 12:14 PM | |
|
Posts: 8171 Rating:
|
New question published by devkumarchandil is split to a separate thread with the subject Want to get some information from one of the ethernet port and send the information to other port. Best regards |
Follow us on