10/25/2012 12:15 PM | |
Joined: 2/15/2012 Last visit: 8/5/2025 Posts: 29 Rating:
|
Thanks, Hamid.Please see atttached. Attachmentfurnace.zip (489 Downloads) |
10/25/2012 1:48 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello again, I have tested the scenario on both PLCSIM V5.4(SP4) and PLCSIM V5.3(SP1).I have not encountered the same problem. My suggestion up to here,Select the integral analog module on the CPU ,then right click and select "Monitor-Modify".See what is the addresses suggested by HW.Config.Try to monitor those addresses via input variables of PLCSIM. If no success up to here, change the addresses to the default addresses suggested by HW.Config.Compile and download them in to PLCSIM. If the problem persists ask SIEMENS via Support Request for possible bugs in that version of PLCSIM. Best regards, Hamid Hosseini |
This contribution was helpful to
1 thankful Users |
2/8/2018 9:16 AM | |
Posts: 5 Rating:
|
I'm having hard time simulating PIW on my program using PLCSIM. I have downloaded the HW setting. Pl see the attachment and suggest ways to resolve.
|
Follow us on