(0)| 2/12/2018 9:39 AM | |
|
Posts: 975 Rating:
|
I have to setup communication from S7 1500 to G120C drives on profinet. I used a free telegram, where speed setpoints - actual values are 32bit. Attached is the telegram configuration. I have some doubts if the 32 bit setpoints - actual values will not cause any problem here, because in the selectable telegrams of the G120C there are no telegrams with 32 bit setpoints - actual values. So, is my telegram configuration ok for G120C? AttachmentCommunication.zip (141 Downloads) |
| 2/12/2018 7:20 PM | |
|
Posts: 1529 Rating:
|
No All telegram words are 16 bit. |
Follow us on