(0)| 3/19/2018 5:09 PM | |
|
Joined: 7/30/2012 Last visit: 1/3/2026 Posts: 335 Rating:
|
Hello I'm using CU320-2PN In that i'm using torque control with encode in vector control mode i need to switch between speed /torque mode using P1501 In speed control i'm using Jog signal to rotate motor but its not working Standard Telegram 2-4/4 In torque control its working fine but facing over speed fault upto some Nm its working fine Before in servo mode i used same logic its worked fine Refer attachments AttachmentTorqueControl.zip (116 Downloads) |
Last edited by: @KB@ at: 3/19/2018 5:30:20 PM |
|
| 3/20/2018 7:38 AM | |
|
Posts: 8092 Rating:
|
Hello, If p1300 is set = 23 i.e. Torque control (with encoder) in vector control type, then change over between speed & torque can not be made. HTH. |
Follow us on