(0)| 3/25/2018 1:57 PM | |
|
Posts: 64 Rating:
|
Dear Friends, I am having a problem with one s7-300 system. The system consists of 313C CPU, four digital cards, and four analog cards. Now three of the analog cards has SF LED glowing. Other analog card doesn't have the SF LED. But the CPU has not any fault /maint LED glowing. Now the digital cards are working properly but the analog cards are not working. I have seen before that if the cards have any fault then the CPU will also show fault. I have checked the wiring and supply voltage to the cards. I am attaching the hardware config & diag as well as photo of the CPU & cards. Please help me to find the solution to run the system without any error. AttachmentHW_DIAG.zip (633 Downloads) |
| 3/25/2018 2:00 PM | |
|
Posts: 64 Rating:
|
AttachmentSYS_PIC.zip (681 Downloads) |
| 3/25/2018 2:18 PM | |
|
Posts: 64 Rating:
|
|
| 3/25/2018 3:55 PM | |
|
Posts: 4620 Rating:
|
Hello RAKIB, did you make any changes to the system or did it suddenly appear? |
| 3/28/2018 1:11 PM | |
|
Posts: 5521 Rating:
|
hi RAKIB, can you show us in a scetch how the modules are wired? have also a look in the manual how the modules have to be wired. hope this helps, regards, |
Follow us on