(1)| 3/25/2018 6:30 PM | |
|
Posts: 5 Rating:
|
I am trying to use a PC Adapter USB to connect PC to KTP600 and download software. But I fail to do so. Choose profibus or MPI both failed. I put as much information as possible into the attached word. Can anyone help me? Thanks
AttachmentHMI connection problem.docx (197 Downloads) |
| 3/26/2018 10:05 PM | |
|
Posts: 199 Rating:
|
Hi, You can take a look to this link Check if the panel is the only device to use the MPI/DP adress "2", if the PG and panel use the same address it's not possible to load the panel, because of address conflict. Regards |
| 3/28/2018 6:23 PM | |
|
Posts: 5 Rating:
|
Thanks guys. I did not expect to receive so many replies... I checked again all the settings inside HMI and TIA, still no problem is found. So I used another USB adapter to have a try and it did work... This is surprising so I used another HMI and computer to try again. What I found out was, I can use 6GK1 571-0BA00-0AA0 to download software to KTP600 basic color DP while if I use 6ES7 972-0CB20-0XA0 then it will fail to find HMI. But I can use 6ES7 972-0CB20-0XA0 to download software to S7-300. So my guess is maybe 6ES7 972-0CB20-0XA0 does not support KTP600 basic color DP? I attached picture of both adapter. AttachmentUSB adapter.docx (182 Downloads) |
| 3/30/2018 5:26 PM | |
|
Posts: 5 Rating:
|
Thank you so much. I ordered one. I will start to test it after I get it. |
Follow us on