(0)| 4/1/2018 8:14 PM | |
|
Posts: 2 Rating:
|
Hello Expert, We are used a Siemens Sinamics G120L (6SL3310-1CE35-8AA0) 315KW VFD which control unit is CU230P-2 DP and power module is PM330L as blower fan. There are used 1 DI as On/OFF, 1 AI (4~20 mA) as speed setpoint and 1 DO as Run feedback. When start command the drive then run drive. After running the drive increase the anlog set value then speed up the drive. Again decrease analog set value then did not speed down the drive but analog value reduced. For kind information, same problem as hand mode. I did not understand that problem. Please help us. With Best Regards Ariful Islam AttachmentFameglas_G120L_315KW.zip (141 Downloads) |
Last edited by: AutoGen_790258 at: 4/2/2018 12:02:40 PMStarter Project is herewith |
|
Follow us on