(1)| 4/3/2018 1:42 PM | |
|
Posts: 64 Rating:
|
Dear Friends, Regards |
| 4/3/2018 4:31 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Rakib; There are links to your first file (MMRR0476.gsd) on the web, associated with an old Bosch-Rexroth unit named HNC100: HNC100 Profibus-DP interface: Connection to Siemens S7 and S5 If this module is the one you would like to insert into your Profibus network then the GSE file is shown in the manual, page 74. You can copy this text into Notepad and save it as MMRR0476,gsd, and then use it in your master's Profibus configurator. I can find no information on your second file, Hein0489.gsd. So Duris's suggestion is valid, provide information on the Profibus slave you are looking to integrate in your network, it would be helpful. If these Profibus slaves are from an older project, either in Step 7 or Com Profibus, you should be able to locate all external gsd files used in the project in the project tree of your software (under a folder simlar in name to ...Data/GSD, and copy them to notepad for insertion in your new project.. Hope this helps, Daniel Chartier |
Follow us on