2/28/2006 1:18 PM | |
Posts: 5822 Rating: (412)
|
Hi, try this Manual: http://support.automation.siemens.com/WW/view/en/1142798 in chapter 3.5 you will find some more information about the possibilities when using the IM 153-2 in a redundant system. Best regards J_Bell. |
3/18/2006 11:55 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318) |
Hi Peters, When there are two IM 153-2 in one active backplain then they are used behind a S7-41xH system or in a configuration with "Software Redundancy". [:o] For the H-System you may find more information in the next link: http://support.automation.siemens.com/WW/view/en/1186523 For Software Redundancy the next link may give some more information to you: http://support.automation.siemens.com/WW/view/en/1137637 Best regards, Late |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on