(0)| 4/28/2018 11:32 AM | |
|
Joined: 7/21/2016 Last visit: 8/19/2025 Posts: 2 Rating:
|
Hi , If anyone is still following this I have created a function block(attached Library1.zip). I haven't done this before so not sure if one can just drag it into a project or not. If you can then it is as simple as placing this FB in your main OB(Make sure the FB is not ticked for Optimised Block Access) and then in the VIJEODESIGNER PLC DIALOG TABLE: select DB(whatever the address of the DB instance once you have compiled the block).DBW0. E.g DB1.DBW0. Function: set terminal clock from PLC and make sure Terminal(HMI) is set to BCD. I am more familiar with Schneider/modicon m340 plc's but have worked on a few s71200/300's. I really appreciate the wealth of information and assistance on the Siemens Online Support. If I can give something back that is great - probably there is a way that is far easier than mine.
AttachmentLibrary1.zip (266 Downloads) |
Last edited by: DaveMorganTechno at: 4/28/2018 11:46:59 AMLast edited by: DaveMorganTechno at: 4/28/2018 11:50:11 AM |
|
This contribution was helpful to
|
|
Follow us on