5/13/2018 5:26 PM | |
Posts: 5 Rating:
|
I am building a CNC router from scratch using basic tools and materials. That machine will be displayed on the Maker Faire in May 25-27, 2018 in Berlin on the Siemens stand. I am using the Apache web server running on the IOT2020 (Installation procedure available in another post) to get a graphical user interface and I will add gcode functionality with a modified grbl source. The detailed build instruction is available on my pages (same as the machine, this page is under construction): https://homofaciens.de/technics-machines-cnc-v3-2-2_en.htm Follow this post to see the build progress and what this machine can do. Hope to see you in Berlin! |
This contribution was helpful to
2 thankful Users |
Follow us on