6/5/2018 10:45 PM | |
Joined: 1/10/2015 Last visit: 8/14/2025 Posts: 47 Rating:
|
Mates, could be IOT2040 also be used as MQTT Bridge for other protocols such as Profinet and Ethernet IP? |
6/6/2018 7:43 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, do you mean to send data via other protocols to the IOT2000 and then send it via MQTT to other devices/cloud? I think this is possible. e.g with node-red. But for now you cannot use Profinet. For Ethernet IP I've found an open source library, but haven't tested it on the IOT2000. But you can use OPC UA or S7 for sending data to the IOT2000. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on