(0)| 6/10/2018 2:51 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello hsnaik; In the configuration of slot 2 (in your screenshot) you cannot have a single range of 128 bytes if slot one is defined with a series of distinct sections. The definition of the screenshot below is that the configuration structures "must be absolutely congruent" between Slot 1 and Slot 2 (same size and type). DP/DP coupler manual : https://support.industry.siemens.com/cs/ww/en/view/1179382 Therefore, Slot 2 should be defined in exactly the same structure as Slot 1, taking into account that inputs of Slot 1 are inverted to outputs of Slot 2 (as you have tried to do). So: Slot 1-------------> Slot 2 8 Bytes IN------->8 Bytes OUT 16 Words IN----->16 Words OUT etc... Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/10/2018 2:52:21 PM |
|
| 6/10/2018 8:16 PM | |
|
Joined: 8/7/2013 Last visit: 3/6/2025 Posts: 90 Rating:
|
Dear Sir, I have taken 64 words as input and 64 words as output. Siemens<<-------------------->>Emerson 64 words-------------------->64words 64 words<---------------------64words we both have taken the same frame but here in case of emerson DCS they dont have numberd memory area like us insted they have slots and signals. e.g When I insert frame of 64 word my hardware will show me the numbered area,in this case Q620...747 and I620...747. Now of this memory area I can make words,bytes bits or Double words. like I620.0,Q700.0....,IW 620,QW700 ,ID620,QW640.... So i have made this type of words of bytes as per my program requirement like for valve status to dcs I am using Q620.0 and for motor current I am using QW500... And in case of emerson DCS the name is SLOTS.. Here they are having 1 slot of 64words configured as input and 1slot of 64words configured as output from GSD provided by us and in that slot instead of memory area like us they have to insert signals. Siemens-------------->Emerson Q620.0 . . QW630------------------> 1 signal of 16byte. Here I am able to send that Data to Emerson correctly as thay have exectly replicate the signals as per my configuration. now when they want to send data to us, i have considers all my input signals as bits means for I620...747 it will become I620.0 to I747.7. but as this didn't work. we have done following.. Siemens ---------------------->Emerson 64words------------------------>Slot1(64words)In that they have set their signal as per my output(shownabove) Siemens <----------------------Emerson 1Byte <--------------------------Slot2(1Byte) Still they are not able to send data to us.while our data is getting received by them perfectly. I hope i have explained my issue properly
|
Last edited by: hsnaik at: 6/10/2018 9:27:20 PMLast edited by: hsnaik at: 6/10/2018 9:30:53 PMLast edited by: hsnaik at: 6/10/2018 9:33:12 PM |
|
Follow us on