(0)| 6/17/2018 11:55 AM | |
|
Joined: 5/31/2012 Last visit: 10/23/2025 Posts: 23 Rating:
|
Dear all i have control unit (CU240E) with following part no : 6SL3244-0BA10-0BA0 from while i upload the attached program from CU240E and then when try to download this project i face the following problem 1- i get following message (Value rejected, Parameter P1080 could not be set to this value) and notice the value of (P1080) changed from setting value in the project which equal = 56.91 HZ to 25 HZ and get alarm on compressor controller which connected to CU240E using USS protocol so what change when i download the attached program ? note : the compressor controller is ATLAS COPCO controller AttachmentSinami_1.zip (230 Downloads) |
Last edited by: Maged Saad at: 6/17/2018 12:06:44 PM |
|
| 6/17/2018 1:37 PM | |
|
Posts: 8092 Rating:
|
Your drive is in fault mode F01023, try by switching OFF & ON power of drive + PLC. If the problem persist I suggest you to contact Siemens or OEM. HTH. |
Follow us on