(0)| 6/6/2011 3:08 PM | |
|
Posts: 21 Rating:
|
Is there any example of VBScript communication with Sinamics? |
| 6/6/2011 3:48 PM | |
|
Posts: 63 Rating:
|
Hi, Pl find attach of eample of VB script eamples for drive. AttachmentVB_Script_Sinamics.pdf (401 Downloads) |
| 6/7/2011 2:38 PM | |
|
Posts: 344 Rating:
|
There is an example project for communication to Micromaster & Sinamics G110 from a PC via Microsoft VB Script. It is under the following link, but it is an internal document. Which means, Siemens wants you to contact you local representative/partner, so they can provide this documentation for you and help you out with it a bit. A hotline may be able to provide this documentation as well. |
| 12/10/2015 8:55 PM | |
|
Posts: 8 Rating:
|
and that link is ????? from :There is an example project for communication to Micromaster & Sinamics G110 from a PC via Microsoft VB Script. |
| 12/11/2015 6:36 AM | |
|
Joined: 5/12/2006 Last visit: 1/20/2026 Posts: 22829 Rating:
|
if you klick on the read marked "link"in the post above you redirectetd to: Regards Christoph |
| 6/22/2018 5:44 PM | |
|
Posts: 4 Rating:
|
It is seams to be gone... can I have copy please? Rick |
Follow us on