(1)| 2/16/2018 5:27 AM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36467 Rating:
|
Under SIMATIC PCS 7 ES/OS System Components Updates, there is also a link for Hotfix 2 for STEP7 V5.6. 1 Innovations and Changes Compared to Earlier Versions 1.1 What has Changed Compared to Version STEP 7 V5.6? Installation •If after installing a hotfix for STEP 7 V5.6 the original installation is changed with "Change program" or "Repair program" the hotfix needs to be installed again. HW Config •In a configuration that uses the function "Use different method to obtain IP address" there is no longer a warning relating to the NTP server address and another subnet. SIMATIC Manager •As of this hotfix: The display of the object size of objects larger than 2 GB has been improved. Report System Errors •A battery fault is also displayed for |
Last edited by: Jen_Moderator at: 2/16/2018 11:56:05 AMOptimized link. |
|
This contribution was helpful to
|
|
| 6/25/2018 6:39 AM | |
|
Joined: 2/9/2015 Last visit: 8/10/2023 Posts: 4 Rating:
|
Pleae, could you enter the link to download the HF 2? |
| 6/25/2018 1:46 PM | |
|
Joined: 10/26/2011 Last visit: 1/13/2026 Posts: 766 Rating:
|
Hello ixo65, this page was replaced by pages, which provides the updates for each Please refer the following forum post, which lists all download pages: You find also all download pages on the PCS 7 overview page |
Last edited by: Thunderstorm at: 6/25/2018 1:48:15 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to
|
|
Follow us on