(0)| 6/15/2018 8:25 AM | |
|
Posts: 6 Rating:
|
I have exactly the same problem and no solution. step7 v5.6 windows 10 1708. When connected to the domain network, step 7 can open project (locally stored on the computer) but as soon as the cable is disconnected, there is no possibility to open any project. This is a big issue as it happend when one of our technician was fixing an issue at a costumer's place. Something I noticed tho is that if you close step 7 but don't close the program, when you reopen it, you can still work on it. Of course saying "you should try to reinstall completely the computer to fix the issue of one program out of 30 that isn't working correctly but is annouced as compatible with windows 10 pro" is NOT an option. I hope someone find a fix to this issue. ------------------------------------------------------------------------------------------ |
Last edited by: SylvainF at: 6/15/2018 9:21:50 AMLast edited by: Jen_Moderator at: 6/18/2018 9:38:10 AMNew subject after splitting |
|
Follow us on