7/23/2018 1:43 PM | |
Posts: 162 Rating:
|
Try using SFB4/5 TON/TOF delays rather than timers that requires timer ressources, it will be easier to handle. |
7/23/2018 1:48 PM | |
Posts: 2826 Rating:
|
Please could you mention: + which PLC (including firmware) + which timer type (S5Timer vs IEC_TIMER) |
7/23/2018 3:14 PM | |
Posts: 2826 Rating:
|
A hand-over like you describe is possible, but I have a counter offer. Consider changing "Function" to an FB and have the timer inside. Attached is what is available for S7-1500 FW2.5 under Step7 V15. Attachmentbasic on references.pdf (343 Downloads) |
Last edited by: #dP at: 7/23/2018 3:24:10 PMadd attachment |
|
7/23/2018 4:49 PM | |
Posts: 17 Rating:
|
Hello DP, Thanks for the suggestion, what you have done works also. I did some trials and solved my problem. I have attached the solution, Regards, |
7/23/2018 4:59 PM | |
Posts: 2826 Rating:
|
Did you use a parameter instance? AttachmentExample of the use of parameter instances.pdf (383 Downloads) |
Follow us on